10/2/2015 6:21 PM | |
Joined: 9/23/2005 Last visit: 12/8/2023 Posts: 4284 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
Many applications demands that some screens objects (IO field, Symbolic IO field, etc.) represents alternately different field objects.
The absolute indirect addressing feature permits that a HMI tag could be “linked” with different PLC tags according references tags.
It is easy to use this feature, despite it just works with non optimized PLC tags (an absolute address is necessary).
Requirements: WinCC BasicV13 SP1.
Project with a minimum configuration (stop button, tags, etc.).
Configuration main steps:
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
Application and tools Demo projects for HMI operator panels under WinCC V13 (TIA Portal) for Basic Panels (2nd generation) and Comfort Panels https://support.industry.siemens.com/cs/br/pt/view/96003274/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Images: Due a size/ format restrictions, the images are first compacted with 7z format (images.z7) and after that attached to a zip archive (data.zip).
Project: Due a size/ format restrictions, the project are first compacted with 7z format (project.z7) and after that attached to a zip archive (data.zip).
AttachmentData.zip (330 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
4 thankful Users |
Follow us on