10/2/2015 2:45 PM | |
Joined: 9/23/2005 Last visit: 12/6/2023 Posts: 4282 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
Many applications demands that the controller select (change) the HMI operation screen. In this simple sample are showed two methods: by function set to controller tag change event and by job mailbox.
Requirements: WinCC Advanced V13 SP1.
Project with a minimum configuration (stop button, tags, etc. See references “WinCC Advanced V13 SP1 – Simple Sample: stop run-time application” ).
Configuration main steps:
by function set to controller tag change event
by job mailbox
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
Application and tools Demo projects for HMI operator panels under WinCC V13 (TIA Portal) for Basic Panels (2nd generation) and Comfort Panels https://support.industry.siemens.com/cs/br/pt/view/96003274/en
Project: attached the project as project.zip.
AttachmentProject.zip (527 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
8 thankful Users |
Follow us on