10/2/2015 8:46 PM | |
Joined: 9/23/2005 Last visit: 11/19/2024 Posts: 4353 Rating: (1454)
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
Many applications demands that some screens objects (IO field, Symbolic IO field, etc.) represents alternately different field objects.
The symbolic array indirect access feature permits that a HMI tag could be “linked” with different PLC tags according references tags.
It is easy to use this feature.
Requirements: WinCC BasicV13 SP1.
Project with a minimum configuration (stop button, tags, etc.).
Configuration main steps:
References: Manual WinCC Professional V13.0
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
Application and tools Demo projects for HMI operator panels under WinCC V13 (TIA Portal) for Basic Panels (2nd generation) and Comfort Panels https://support.industry.siemens.com/cs/br/pt/view/96003274/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Images: Due a size/ format restrictions, the images are first compacted with 7z format (images.z7) and after that attached to a zip archive (data.zip).
Project: Due a size/ format restrictions, the project are first compacted with 7z format (project.z7) and after that attached to a zip archive (data.zip).
AttachmentData.zip (468 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
9/16/2017 12:25 PM | |
Posts: 9 Rating: (0) |
And in this case what is the correct way of adding multi dimensional array to HMI? Like array [0..5,0..15] of Data type? |
Follow us on