Industry Online Support
Technical Forum
11/21/2007 3:37 PM | |
Joined: 9/17/2007 Last visit: 4/17/2023 Posts: 799 Rating:
|
Hello, 1.) sorry for my english...but i´ve gotno other choice... 2.) my problem: we installed an WinCC - system like this: - 1 WinCCServer; Simatic Rack PC IL 43(Win 2003 server R2 with simatic multilanguage interface) - 3 WinCC clients - without own packages (nodistributed system with several servers) In this project, we use a script to write values from anuser archiv (this work as replacement for acombo box)in an otheruser archive (here we collect all informations). These script we have writtenstrictly like the instructions in WinCC-Information-System.If we test these script one time, or fifty times, or hundred times (its different)it works well, but suddenlythe scriptcrashes... (and then no other script starts...the winCC RT surfaceisunusable from these moment...) (but other applications works fine on thesesystem, no deadlock...) Thescreen displays the message"error in ntdll.dll - access violation on adress xyz..." InApDiaglogI found the information, that user archive can´t open (or an other error, yesi knowerror no define in ccuacapi.h),but theaccess - handling of user archives in an WinCC internal... and dosen´t work correct. (remark: the cause of the crash is always in connection with WinCC - user archiveshandling) Any suggestion will be very appreciated. Best regards, vanDyk Attachmentdiagfiles.zip (35 Downloads) |
Last edited by: vanDyk at: 21.11.2007 15:44VG / regards vanDyk |
|
11/21/2007 4:22 PM | |
Posts: 145 Rating:
|
Hi, Which WinCC version are you using? Windows 2003 server R2 is not compatible with WinCC V6.0 Sp4 or earlier. with Regards |
Follow us on