3/9/2020 12:16 PM | |
Joined: 7/14/2016 Last visit: 9/12/2023 Posts: 387 Rating: (27) |
Dear experts, I am doing server client configuration in Wincc and I read this manual. Manual differentiates between two cases: - Multi user system, where there is only one server with multiple clients. - Distributed system, where there are multiple servers, each may have different tasks and client can access all the servers as required. The difference in both configuration procedure is also given on pg-14,15. My questions are: 1. What is the difference between two procedures? they look same to me. 2. Does multi-user means client without own project and distributed means client with its own project? 3. In case of client without own project how do I start runtime in client or Import server data? 4. How do I decide which is suitable for me? I have one server one client and client has same functionality as server. Thanks in advance, Kbv. |
Last edited by: Kbv at: 03/09/2020 12:18:22Last edited by: Kbv at: 03/09/2020 12:18:49Don't just think in terms of solutions... |
|