Industry Online Support
Technical Forum
2/20/2008 12:32 PM | |
Posts: 1275 Rating: (123)
|
Hi, First of all, you can upgrade your system for free to v6.0 SP4. Just be sure to check compatibility with other Siemens software which are installed on that computer, and upgrade the ones you can. To prevent changes you should prevent the operator's access to WinCC Explorer... and to Windows as well... you should block the "Alt + Tab", "Ctrl + Alt + Del" and other key combinations on "WinCC Explorer" -> "Computer" -> "Properties", under the "Parameters" tab. All buttons which open Windows Explorer, WinCC Explorer, etc. should be protected with a password. Finally, you should use the "Autostart" funcion (on the Windows Start menu, access "Simatic" -> "WinCC" -> "Autostart"), to make sure that WinCC starts as soon as Windows start (with this, you won't have to start WinCC automatically, and WinCC Explorer will be closed while the system is under operation). Best regards, Danielle |
5/2/2008 9:24 AM | |
Posts: 1084 Rating: (72)
|
Never tought of that one , good one. You are sure you can not open the wincc explorer in that way? with regards, Ikkezelf |
Follow us on