Industry Online Support
Technical Forum
5/22/2007 7:35 PM | |
Posts: 8 Rating: (0) |
Hello, I'm trying to link a new WinCC aplication with an old S5 CP535. I have do it before with an S7400 an a lot of work in the data header. But now it doesnt work. I think the problem can be that in the CP535 i must configure de interface number and job number of each job, either in the local side and the remote side. This was able with Coros but not with WinCC. I have configured two links: FETCH (active at the WinCC side [SSNR 0, ANR 1]and passive at the PLC side [SSNR 0, ANR 1]) WRITE (active at the WinCC side [SSNR 0, ANR 2]and a passive RECEIVE at the PLC side [SSNR 0, ANR 2]) Is this correct?? I think its possible because ia have read it in this posts: /tf/WW/en/Posts/2072/tf/WW/en/Posts/1301 Thanks a lot!!! |
5/22/2007 7:57 PM | ||||||||||||||||||||||||||||||||
Posts: 1275 Rating: (123)
|
Hi JaviM, I see you've already posted here too.. Actually I've never worked with WinCC + S5... Check this FAQ. Here's some stuff I've found, from Nemo's previous posts: As far as I know, you can use in WinCC the S5-Channel, which is a WinCC Add-on. You can get more Informations here: http://www.industry.siemens.com/itps/it4industry/en/wincc/index1503863.htm Whether your CP is running with this driver, should you check with the it4industry-people. You should contact the WinCC Competence Center in Erlangen, which is supporting and developing the S5-Channel. http://www.industry.siemens.de/IT4Industry/EN/SOLUTION_SERVICES/SIMATIC_ADDONS/KANAL_DOWNLOAD.HTM
Also... post your diagnose folders... Best regards, Danielle |
|||||||||||||||||||||||||||||||
Follow us on