3/27/2015 12:22 PM | |
Posts: 10 Rating: (0) |
hello in wincc explorer please i want a way to save imcoming alarm to file text thank you |
3/30/2015 7:45 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello youssef 2013, where do you get an error, during compilation in the C-Editor, or during Runtime ? In the attachments you find as script-example, which can be compiled succesfully, you have to modify it for your special use. Regards Georg Berghof AttachmentGMsg_Mod.txt (478 Downloads) |
Last edited by: bg2492 at: 3/30/2015 7:46:36 AMPS: If this post did really help you, you may use the Rate-button |
|
3/31/2015 9:31 PM | |
Posts: 10 Rating: (0) |
Heloo Georg Berghof thank you very much sir for your help and your reply for the function GMsgFunction is worked for me when i add it in button i create a new picture i added a control alarm i add a checkbox with 4 , i added button and a static text i ceated an internal tag "testing" to test 4 alarm messages with diferrent text and priority when i cheked box 1 i get message alarm n1 from tag "testing" .... i created an internal tag " MsgNr " for saving the number of the alarm coming i added this code in button , and when i checked the box i get alarm message and the static text give me the number of message, the function it worked for me , now i can resolve the error of c editor my question is when i delete the function GMsgFunction from c-editor and from the button ,the picture still worked and i get the number of message, i insert the code to save message incomming in filetext doesn't work iinsert the code to save message incomming in internal tag ,doesn't work i wish to know if i can save the message in internal tag and how i can read it using for example static text thank you the code i insered in button is joined AttachmentGMsgFunction_button.txt (260 Downloads) |
4/30/2015 7:33 PM | |
Posts: 10 Rating: (0) |
hello
thank you |