3/13/2017 10:35 AM | |
Joined: 8/3/2009 Last visit: 3/27/2025 Posts: 15107 Rating:
|
Hello Willdark In the most cases you do not need Simatic Net Installation. only if you use a special Simatic NEt Product like OPC Server, WinAC. If you have configured the connection correctly in your Project then you only have to set the PGPC interface on the Runtime System. But you could everything check in the following FAQ: https://support.industry.siemens.com/cs/ww/en/view/24109937 I would use a HMIStation without Component configuration. Another Hint to the Configuration with a S7 CP: - you have to set the Slot number of the CPU not of the CP!!! but the IP Adress of the CP!! Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/15/2017 10:50 PM | |
Posts: 9 Rating:
|
Towome Thanks for your appreciated help. Willdark |
Follow us on