Industry Online Support
Technical Forum
2/18/2010 6:25 PM | |||||||||
Posts: 27 Rating: (0) |
Hello experts I have this MP277 link to an Ethernet network. On the same network I have a standard PC with Windows XP. I have made a share on Windows XP with the security on the share and the folder set to Everyone Full Control. Now I instruct the MP277 to put his recipe file on the share. I use the net use command in the prompt level of the MP277 to create a path to the PC that I call PC. So in the recipe properties I call the recipe to be on \\network\PC. I can compile download and everything works fine. But when I go on the page that has the recipe view there is a message at the bottum of the recipe view "Error,, Action Aborted!". In the MP277 miniweb system Diagnostics I see:
I try in an Windows Explorer inside the MP277 and I can create files without problem. Any Idea on why and if I can put the recipe outside the MP277? The ultimate gool is to share a recipe between the PC and the MP277. Any help appreciated.... |
||||||||
2/24/2010 9:46 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, did you enter the name from the panel into the "lmhosts file"? Look into this FAQ -> http://support.automation.siemens.com/WW/view/de/13336639 (table 1 ,point 3) regards, |
2/25/2010 4:31 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, i also have saved recipe files via Ethermet to a PCfor a longer time ago and its works fine. An idea: You can use a "Thin Client" solution or a solution via Sm@rtAccess. You have the recipe on one PC/Panel and all other devices "look" on this PC/Panel. regards, |