4/30/2010 10:04 PM | |
Posts: 27 Rating:
|
Hello |
5/5/2010 1:13 PM | |
Joined: 4/29/2010 Last visit: 12/4/2023 Posts: 1557 Rating:
|
Hello, wich device do you use in this case, a panel or a pc-runtime? Best regards. |
4/16/2014 10:07 AM | |
Posts: 1 Rating:
|
I have the same problem. Config : - MP277 8" Touch - WinCC Advanced Version V11 SP2 Update 5 |
4/17/2014 3:12 PM | |
Joined: 2/15/2011 Last visit: 12/6/2023 Posts: 13 Rating:
|
Regarding that trend I dont do that any more. I use a DLL called vbSendMail.dll. http://www.freevbcode.com/ShowCode.asp?ID=109 In the WinCC Scipting, i just do a scipt using that dll. It works for me with WinCC on windows xp, 7, and 8. I never tryed it with a panel but you can try. Respond if it works or you need more information. |
Follow us on