Industry Online Support
Technical Forum
10/14/2008 9:37 AM | |
Joined: 4/24/2006 Last visit: 9/14/2023 Posts: 8592 Rating:
|
Hi, When you are using WinCC flexible 2007, the image of MP370 is v7.2.0.3 When you use WinCC flexible 2008 it will be v7.2.1.0 See also this link: http://support.automation.siemens.com/WW/view/en/21742389 Unfortunately wincc flexible 2008 isn't mentioned When you want to use WinCC flexible 2008 to download project, you should use image v7.2.1.0 Please perform an OS update if necessary Best regards, Wizard |
Follow us on