3/4/2011 12:02 PM | |
Joined: 12/20/2008 Last visit: 4/19/2024 Posts: 19 Rating: (0) |
Dear All, I am facing a problem with my WinnCC Flexible 2008 sp2. When I try to open a WinnCC project by pressing the page icon in STEP7 enviroment, the bar graph starts to run, arrives to 100% but Wincc flexible does not run. (see attached file page1). Out of STEP7 enviroment, i press the icon on my desktop, the flag of WinCC flexible start to run but after 5 seconds i see that has stop to charge. I can also wait an hour but does not happen anything (see attached file page2). Can you please help me to solve the problem? I thank you very much Attachmentpage 1 plus page 2.pdf (208 Downloads) |
Last edited by: Pier7o at: 3/4/2011 12:08 PMLast edited by: Pier7o at: 3/4/2011 12:06 PM |
|
3/4/2011 3:05 PM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136)
|
hello Pier7o, please try to reset wincc flexible. here some informationsto dothis... http://support.automation.siemens.com/WW/view/en/36645252 regards Manfred |
3/7/2011 9:09 AM | |
Joined: 12/20/2008 Last visit: 4/19/2024 Posts: 19 Rating: (0) |
Dear Manfred, I have tried to reset it by following the instruction concerning the Flexible 2008 ( as i have got) but after 4 seconds it stops.
Do you think i can follow the other procedure for the previous versions? I thank you in advance. Pier AttachmentImmagine.pdf (152 Downloads) |
3/7/2011 9:55 AM | |
Joined: 12/20/2008 Last visit: 4/19/2024 Posts: 19 Rating: (0) |
Hi Umencho, yes suddenly... Rgds |
3/7/2011 10:42 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
So my suggestion is reainstall Flex... |
10/17/2011 4:14 PM | |
Posts: 3037 Rating: (192)
|
Hello, You should reset WinCCflexible. Here is the FAQ for this. Tweety |
Last edited by: Tweety at: 10/26/2011 10:42 AM |
|
9/30/2015 10:25 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Mehr Shah is split to a separate thread with the subject WinCC Flexible 2008 SP3 stopped. Best regards |
Follow us on