11/29/2024 10:36 AM | |
Joined: 7/19/2022 Last visit: 4/23/2025 Posts: 436 Rating:
|
Hello DamianQS, With the TIA Portal TRIAL license, you can configure WinCC panels as well. Is this license in use? Attached a screenshot of the ALM |
Last edited by: JBS98 at: 11/29/2024 10:36:37If this Information really helps, you could use the Rate function |
|
11/29/2024 10:36 AM | |
Joined: 8/6/2018 Last visit: 4/25/2025 Posts: 366 Rating:
|
Hello, What error does it have when you open it? Could you tell us which HMI you use? Thanks you |
11/29/2024 10:41 AM | |
Joined: 8/12/2021 Last visit: 4/11/2025 Posts: 351 Rating:
|
Hi! Which panels do you want to see in the project? Tia Portal Professional comes with WinCC Basic, but there are more options that allow programming depending on the panel type. Check the information in the following link (Product Information tab).
|
If this Information really helps, you could use the Rate function |
|
Follow us on