7/17/2013 6:41 AM | |
Joined: 9/16/2011 Last visit: 6/20/2024 Posts: 291 Rating: (6) |
TCP/IP Dear White Snoppy, Do try the following steps: 1. Open your Wincc project 2. under tag management, right click on TCP/IP. and select "system parameter" 3. click on "unit" tab 4. In the drop down menu of "Logical device name". Check what Ethernet card is selected. It should be the same, as to which you connect your Ethernet cable, otherwise change the selection in the "System parameter" Check the attachements ! Reg, Ashish
Attachmentattachment.pdf (536 Downloads) |
Reg, |
|
This contribution was helpful to1 thankful Users |
7/17/2013 7:31 AM | |
Joined: 4/17/2012 Last visit: 6/17/2024 Posts: 474 Rating: (10) |
Hi, i think runtime you can monitor parallel two system only i think so. if you disconnect any one system and check it |
7/17/2013 6:06 PM | |
Posts: 33 Rating: (0) |
Of course I did all this things. Is not my first time with WinCC. One thing puzzles me. Why I dont have TCP/IP - > before my network card name |
Follow us on