7/17/2008 8:29 PM | |
Posts: 2661 Rating: (279) |
We are using WinCC 6.0 but it should work with V6.2 as well. Find attached the runtime account settings we are using. You are right about the DCOM settings. Changing these is not good. The manual specifically states that all the settings (after WinCC & connectivity pack installations) are ok. In fact when we were commissioning this (about 2 years ago), I had to restore original image of WinCC client machine since we messed with the DCOM settings and the thing stopped working! First you should make sure the OPC communication is ok by trying with a “test” OPC client (available free on the web).
AttachmentDokument1.pdf (364 Downloads) |
7/18/2008 4:08 PM | |
Posts: 2661 Rating: (279) |
Settings as attached. Regards AttachmentDokument1.pdf (364 Downloads) |
Follow us on