7/21/2014 7:08 AM | |
Posts: 1299 Rating: (136)
|
Hello, you have to use the same windows user on server and client pc. K!ke |
7/21/2014 6:11 PM | |
Joined: 5/19/2009 Last visit: 7/30/2024 Posts: 40 Rating: (0) |
I've tried with the same user name and password, but nothing changed. In the attachment are two pictures, theone that shows the error and the other that shows that the client PC can see and remotely access the server PC. Does anyone have any ideas? Regards, Igor AttachmentWinCC_Client.zip (204 Downloads) |
7/22/2014 12:13 PM | |
Joined: 5/19/2009 Last visit: 7/30/2024 Posts: 40 Rating: (0) |
Here is the project (developed in TIA V12 SP1). This one I've created this morning, and i got the same error. I just don't see what I'm doing wrong. I can activate and deactivate the project from WinCC Client PC using Simatic Shell. Furthermore, while the project is running on the server PC, with WinCC RT Start i can browse the server to choose the .mcx file of the project. When I select it, the pop up for login appears and I log in. The WinCC starts and after that i can the error message. I have the same user name and password on both server and client PC (both are running Win 7 64-bit Pro) and all users are in the SIMATIC NET group. AttachmentSERVER_CLIENT.zip (174 Downloads) |
Follow us on