8/6/2016 12:23 PM | |
Posts: 73 Rating: (1) |
I have installed the following softwares so far: WinCC TIA V13 WinCC professional V13 STEP7 TIA V13 PLCSIM V13 STEP7 TIA V13 SP1 WinCC TIA V13 SP1 PLCSIM V13 SP1 Now I want to install WinCC professional V13 SP1. It goes fine until the end when prompting an error that there were errors during the setup, then suggesting me to restart. After rebooting, my TIA starts fine, but it can't simulate, particularly, my HMI devices (including WinCC RT). I tried to repair WinCC Professional SP1 with and without my anti-virus on. It concludes with the same error that there are errors during the installation. AttachmentSIA_WINCC_PROFESSIONAL_V13_SP1@16-08-06_01-27-44_summary.txt (49 Downloads) |
Last edited by: moghimian.s at: 8/6/2016 12:43:05 PM |
|
8/10/2016 5:09 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (194) |
Hello moghimian.s, I don't know, if this is the cause of your problem, but the following FAQ states, that you have to install STEP 7 first and WinCC afterwards. In which order did you install your software?
Did you check that there is no older, not parallel compatible software on the System?
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
8/27/2016 9:42 AM | |
Posts: 73 Rating: (1) |
I don't know how it got resolved, now. I just tried installing advanced RT. Anyways, thank you for your answer. |
Follow us on