10/5/2015 5:46 PM | |
Joined: 12/13/2011 Last visit: 4/19/2023 Posts: 123 Rating: (14) |
I have not adjusted the tag scan rates, I have only messed with the scan rate of the screens themselves. |
10/5/2015 7:56 PM | |
Joined: 12/13/2011 Last visit: 4/19/2023 Posts: 123 Rating: (14) |
I have added a video of the issue. Every time I change the screen the animations flicker from their default (configured) state to the current state from the PLC. I have the screens refresh rate set to 250 ms, how can I match the scan rate to the tags?
Attachmentflicker5.avi (137 Downloads) |
Follow us on