2/12/2025 3:00 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello rorshack you could try to reset all temp HMI files and generate completley new, perhaps there is an incosistency in the project: https://support.industry.siemens.com/cs/de/en/view/109778709 If this is not the reason, therre has to be some error in your project... if the connection and also the tagnames are different then it cannot be that the value is written to wrong datapoints. I think then there is something wrong in your HMI programming Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on