10/3/2015 12:14 PM | |
Joined: 9/23/2005 Last visit: 9/29/2023 Posts: 4241 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
Access restrictions based on Users limits the user to perform buttons commands depending of his authorizations. It could be used for several targets (like to block access to screens). In this example, depending of logged user (John, Steve, Lewes, Bill) it is possible to change tags (by button or IO field).
The principle is: 1 – Actions (e.g. Buttons and IO field) are linked with authorizations definitions 2 – User groups defines typical case of users and these respective authorizations 3 – User are defined and linked to User groups
User ↔ User Group (set of Authorizations) ↔ Authorization ↔ object access restriction
Logon dialog is called by button.
The users could be managed online by User View object (the features are limited conform the user authorization settings).
Requirements: WinCC Professional V13 SP1.
Project with a minimum configuration (stop button, tags, etc.).
Configuration main steps:
Optional: manage online User / Password
Note: in this example, just the Administrator user can manage all users.
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Images: Due a size/ format restrictions, the images are first compacted with 7z format (images.z7) and after that attached to a zip archive (data.zip).
Project: Due a size/ format restrictions, the project are first compacted with 7z format (project.z7) and after that attached to a zip archive (data.zip).
AttachmentData.zip (218 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
3 thankful Users |
4/20/2016 9:46 AM | |
Joined: 8/21/2014 Last visit: 9/14/2023 Posts: 733 Rating:
|
New question published by anayisse is split to a separate thread with the subject Using a passwort when navigating between views. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on