10/3/2015 1:04 PM | |
Joined: 9/23/2005 Last visit: 12/1/2023 Posts: 4279 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
In this simple sample, a x y trend is displayed on HMI start screen is showed in two versions: as real time trend and as historical data.
Three variants are showed:
Requirements: WinCC Professional V13 SP1.
Project with a minimum configuration (stop button, tags, etc. See also “WinCC Professional V13 SP1 – Simple Sample: Trends“ https://support.industry.siemens.com/tf/br/en/posts/135199/ ).
Configuration main steps:
Real time X Y Trend:
Historical data (Logging Tags – Cyclic) X Y Trend:
Historical data (Logging Tags – Cyclic selective) X Y Trend:
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Images: Due a size / format restrictions, the images are first compacted (images.zip) and after that attached to a zip archive (data.zip).
Project: Due a size / format restrictions, the project are first compacted (project.zip) and after that attached to a zip archive (data.zip).
AttachmentData.zip (412 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on