8/31/2018 10:46 PM | |
Joined: 6/5/2016 Last visit: 4/9/2025 Posts: 2 Rating:
|
Hello! Maybe someone can help me out or has the same problem. I am working on a TIA V14 Professional and try to create a dynamic text list with strings, which are located on the plc. Did the exactly same thing in a Advanced and everything was working fine. But in the Professional version the pop-up, where i can select to use a parameter instead of the static text, is not showing the option for this. I tried to the the exact same thing as in this article https://support.industry.siemens.com/cs/ww/en/view/57025748 The strange thing is, i cannot select a wstring as my string variables in the plc are strings indeed. Hope someone can help me. Thanks. |
Last edited by: Jen_Moderator at: 9/3/2018 10:21:16 AMOptimized link. |
|
Follow us on