9/18/2020 7:53 PM | |
Joined: 6/25/2015 Last visit: 3/21/2025 Posts: 4 Rating:
|
Hi all, I too have a problem with WInCC Professional v15.1 Whenever I try to download a SCADA project to a file system I get no output data. I can specify a folder where the files should be exported. I tried several foldes so far, nothing works. There are no errors during the compilation and WinCC claims that "Loading completed (errors: 0; warnings: 0)". What could go wrong? I am doing this from a physical machine who solved the problem? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: xodus at: 09/18/2020 19:55:13Last edited by: The Helping Hand at: 09/21/2020 12:11:02New subject after splitting |
|
9/29/2020 10:42 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello do you want to load into the Runtime PC then look at: https://support.industry.siemens.com/cs/ww/en/view/88780011 If you want to load in the local file System then look at : https://support.industry.siemens.com/cs/ww/en/view/103198851 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on