9/22/2022 12:58 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello JV do you work with the latest Update in TIA V17? https://support.industry.siemens.com/cs/ww/en/view/109784441 Bye Murof |
If this Information really helps, you could use the Rate function |
|
9/22/2022 1:10 PM | |
Joined: 1/21/2013 Last visit: 4/19/2025 Posts: 3765 Rating:
|
Hi JV., you should verify, your SVG file is okay. You can do this using the W3C Markup Validation Service. I also made very good experiences in using the SVG Optimizer. If the error still occurs, you can use the Export Graphics Tool to export the graphics from the "Graphics Collection" and test the Siemens SVG. Kind regards |
This contribution was helpful to
1 thankful Users |
9/23/2022 6:44 AM | |
Joined: 4/1/2020 Last visit: 5/25/2023 Posts: 6 Rating:
|
Hello Murof, Will try optimizing it with Inkscape. I'm not sure what you mean with checking the header actually, I'm not so into the svg files. Hello Stefan, I do see them both in engineering and in the runtime. Here's a link to the svg file. [snip] Attachment11.zip (161 Downloads) |
Last edited by: Jen_Moderator at: 09/23/2022 09:59:49Link removed and file added as zip file. |
|
9/23/2022 11:28 AM | |
Joined: 1/21/2013 Last visit: 4/19/2025 Posts: 3765 Rating:
|
Hi JV., the SVG file is valid, but it has a lot of - let's call it - "open paths". I mean there are path elements inside which are not for one continuous path, they contain multiple paths. Maybe that's the reason of the issue. Where is the file from? How was it created? Maybe, the creator can provide a better version. Of course, you can also create a support request to ask Siemens. Kind regards |
This contribution was helpful to
1 thankful Users |
9/23/2022 12:07 PM | |
Joined: 4/1/2020 Last visit: 5/25/2023 Posts: 6 Rating:
|
Hello Stefan, The file is originally a DWG file, which is opened in adobe illustrator and exported as SVG. |
9/26/2022 6:12 AM | |
Joined: 1/21/2013 Last visit: 4/19/2025 Posts: 3765 Rating:
|
Hi JV., I would suggest you to edit the image and simplify the paths. Kind regards |
Follow us on