12/23/2020 3:53 PM | |
Joined: 2/6/2015 Last visit: 4/24/2025 Posts: 80 Rating:
|
Hi Diegomb, Yes, you can work with a V14.1 project in V15.1. When you will open your project in V15.1 the project will be migrated to V15.1 but the firmware will not change. This is optional. About as you could do a backup I would recommend look this FAQ: How do you do a data backup of the WinCC Project (WinCC V7 and WinCC Professional) on the Operation Station (OS)? https://support.industry.siemens.com/cs/ww/en/view/109766573 Best Regards, CGA81 |
If this Information really helps, you could use the Rate function |
|
12/23/2020 7:38 PM | |
Joined: 12/23/2020 Last visit: 1/12/2024 Posts: 18 Rating:
|
Thank you CGA81. I already red that FAQ but it doesn't explain how to restore the bakup in the runtime system. Is there any pdf that explains this topic for Wincc Profecional and Wincc Advanced? I want to be sure I can roll back to a running project. Thanks. |
Follow us on