2/12/2014 7:46 AM | |
Posts: 1299 Rating:
|
Hello, this depends on your hardware. if your runtime system is a simatic pc you choose this one as hardware and add the runtime system in device view. if it's a generic pc you can do both, either you insert a generic pc and add the runtime component manually or you choose directly the runtime component and it will add the pc automatically. you also need to add a communication module with which your runtime pc will communicate with the s7-300. Here you can find the getting started: http://support.automation.siemens.com/WW/view/de/72927729 K!ke |
2/12/2014 6:24 PM | |
Joined: 6/19/2006 Last visit: 12/7/2022 Posts: 55 Rating:
|
K!ke, Thank you so much for the reply! All the best. The Fro |
Follow us on