4/14/2016 4:13 PM | |
Joined: 3/12/2015 Last visit: 12/18/2024 Posts: 545 Rating: (15) |
Good evening sandy, could you make a screen shot of the process you are trying to do? |
4/15/2016 1:00 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (194) |
Hello SANDY GORASIYA, there are three limits that might cause your problem: The maximum number of I/O-fields per screen is 400, The objects in the faceplate count as objects of the screen. For example: You have 40 I/O fields on your screen and 20 I/O fields in a faceplate. Could that be the issue with your screen? |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
4/15/2016 1:25 PM | |
Joined: 4/28/2015 Last visit: 5/6/2024 Posts: 34 Rating: (6) |
Dear H.J.
but i have seen that if i will copy all object By ctr+A and pest new screen and then i compile it then it work ok. |
Follow us on