4/1/2022 8:15 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello howitzer00 I think WinCC RT Advanced is not released for use on virtualised environment for a productive system. Do you have installed the latest Update for V16 (Runtime and Engineering)? Why do you use only V16? you could also try with latest V17 Version. You should check the system limits in the TIA Portal Help System perhaps the freezes are caused by exceeding systemlimits: https://support.industry.siemens.com/cs/ww/en/view/109798671/143186011019 Bye Murof |
Last edited by: Murof at: 04/01/2022 08:15:39If this Information really helps, you could use the Rate function |
|
4/1/2022 3:54 PM | |
Joined: 5/24/2021 Last visit: 2/22/2024 Posts: 7 Rating:
|
Win 10 Pro 21H2. WinCC RT Adv V16 UPD5. |
4/1/2022 4:16 PM | |
Joined: 7/5/2013 Last visit: 4/17/2025 Posts: 3147 Rating:
|
Hello howitzer, see Delivery release for WinCC V16. WinCC Runtimes are released for "Windows 10 Pro Version 1809 / 1903 (OS Build 17763 / 18362)". What I found is that 21H2 is build 19044. The newer build you are using might cause the issue. Can you try creating VM with one of the named builds and check RT behaviour there? Regards, Frink |
Last edited by: Prof. Frink at: 04/01/2022 16:18:16Added information about build. Pi is exactly three! |
|
Follow us on