8/6/2024 5:59 PM | |
Joined: 6/15/2024 Last visit: 4/17/2025 Posts: 22 Rating:
|
Our version of WinCC is V7.5 SP2 Upd9. Do you mean, Do you mean I have to update WinCC to the latest version? |
8/8/2024 8:52 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello Muksidintaslim the latest Update for WinCC V7.5 SP2 is Upd18 at the moment: (LINK) So it would be an option to reinstall your Upd or go also to the latest one But it should appear automatically after PC start. If not check also the taskbar settings perhaps you have just hidden it Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
9/28/2024 10:08 AM | |
Joined: 6/15/2024 Last visit: 4/17/2025 Posts: 22 Rating:
|
Thanks Murof, after our wincc reinstalled, it seems back to normal again. |
Follow us on