5/17/2023 1:01 PM | |
Joined: 8/3/2009 Last visit: 4/25/2025 Posts: 15355 Rating:
|
Hello murat1290can you usecase is not 100% clear. As I understand, your winCC Professional reads data from the SQL Server (Not WinCC Instance) and thsi you want to show on trend view? In Trend view you can show onlie values and values out of the Tag logging. But this tag logging values are logged by WinCC not from outside. But there is also a possibility to show a trend with external data. Have a look at this link to the WinCC V7 Manual (in WinCC Prof its quite the same): https://support.industry.siemens.com/cs/ww/en/view/109792585/95220468491 Perhaps it helps Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on