5/24/2012 8:30 AM | |
Posts: 19 Rating: (0) |
Picture 2 |
5/24/2012 8:39 AM | |
Posts: 1064 Rating: (72) |
I may be incorrect but the tag is showing as internal and not connected to plc ,is this what you wanted or to change something in the plc ? |
5/24/2012 10:05 AM | |
Posts: 19 Rating: (0) |
ok 3 pictures for you... i cannot connect to the plc using RT Advance or Professional, i was able to do it with a ktp1000 Basic PN.
|
5/24/2012 10:06 AM | |
Posts: 19 Rating: (0) |
Picture 4 |
5/24/2012 10:09 AM | |
Posts: 19 Rating: (0) |
PLC IP 192.168.0.1 PC Station IP 192.168.0.5 same as my desktop pc with TIA + WinCC installed
|
5/25/2012 12:52 AM | |
Posts: 19 Rating: (0) |
i dont know whats happening :( with the KTP1000 is so easy the connection with the PLC |
5/25/2012 1:06 AM | |
Posts: 19 Rating: (0) |
trying to make the same thing as your picture, i created a new connection but still doesn't work 3 pictures ( 7, 8 and 9)
|
5/25/2012 1:08 AM | |
Posts: 19 Rating: (0) |
picture 8 |
5/25/2012 1:14 AM | |
Posts: 19 Rating: (0) |
Picture 9 |
6/1/2012 3:14 PM | |
Posts: 3037 Rating: (192)
|
Hello, Have you a HMI connection from your PLC to HMI? Tweety |
6/4/2012 4:03 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello SSJV, Have a look at this FAQ on How do you configure an S7 connection for the OPC server of a PC station in TIA Portal V11 to access the data of an S7-1200 over Industrial Ethernet? Provide a feedback aftre trying. Still the easy way is to upgrade the firmware of your CPU to v2.2 andcreate a connection directly by specifying the S7-1200 driver in WinCC Professional v11 SP2. |
Like it? Rate it! |
|
6/5/2012 10:24 PM | |
Posts: 19 Rating: (0) |
Firmware 1.0, is that the problem ? do i need to update the firmware ? |
6/6/2012 6:33 PM | |
Posts: 19 Rating: (0) |
thanks for your advice! now, i would like to know where can i buy the update Memory Card ? best regards...
|
6/7/2012 5:52 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello SSJV, Now buying a Memory Card only for the purpose of upgrading the firmware may not help. Hold on for some time till we get some official information. As currently the S7-1200 System Manual (04/2012)says "Note You cannot update an S7-1200 CPU V2.2 or earlier to S7-1200 V3.0 by firmware update." So try to do the firmware update with the help from your local siemens representative. |
Like it? Rate it! |
|
Follow us on