8/22/2016 6:44 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hello, mak a screenshot of installed programs. If you have installed WinCC RT Professional V13.0 SP1 then you can't install a Update for WinCC RT Professional V13.0 because the SP1 is the higher version and you can look here for updates: https://support.industry.siemens.com/cs/ww/en/view/109439573 the latest is UPD9 for V13.0 SP1! Regards |
8/22/2016 7:34 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (192) |
Hello is_razi, I would say it is because WinCC Advanced is a single operator station system and WinCC Professional is a SCADA system. The runtime is dependent on the name of the PC in the device configuration. There might be some more historic reason, too. I'm just guessing here however, sorry. If you use the WinCC RT Simulation in TIA Portal it mostly works exactly like the according runtime for both systems, so you don't really need to build your professional runtime for testing. If you do. don't forget to adjust the PC Name in the project. Here is the download list for WinCC Runtime Professional V13 (without the SP1):
Maybe try an update lower than 6 and have a look if this is can be installed? ... Can you update to SP1? It helps with bugs and stability issues if you keep the TIA Portal updated. |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
8/23/2016 9:59 AM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (192) |
Hello is_razi, no, you understood that wrong, sorry. You have to install the WinCC Runtime Professional seperately. About the second question:
Here is the link to the chapter about the WinCC Professional Runtime in the manual of WinCC Professional V13 SP1. It might be helpful to you if you just want to look up some Details:
|
Last edited by: H.J. at: 8/23/2016 10:06:47 AM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|