8/10/2007 3:55 PM | |
Posts: 37 Rating: (0) |
Dear All , I am facing problem regarding WInCC runtime. Runtime is not getting activated as application is getting hand at 77% only .I have attached some log file & snap shot images. Please suggest me the solution Thanks in advance AttachmentWINCC LOG & ERROR.zip (55 Downloads) |
8/10/2007 3:56 PM | |
Posts: 37 Rating: (0) |
attachment 1oo 5 |
8/10/2007 3:56 PM | |
Posts: 37 Rating: (0) |
attachment 2 oo 5 |
8/10/2007 4:00 PM | |
Posts: 37 Rating: (0) |
save the aatached file using .rar extension as it WinRAR archive file
AttachmentWINCC LOG & ERROR.zip (65 Downloads) |
8/10/2007 4:31 PM | |
Posts: 37 Rating: (0) |
WinCC V6.2.0.1 |
8/10/2007 4:31 PM | |
Joined: 10/26/2005 Last visit: 4/29/2024 Posts: 282 Rating: (48) |
Hi! I had those problems to, but "WinCC_V62_HF5" fixed them Now its weekend off.//Per |
8/13/2007 3:50 PM | |
Posts: 37 Rating: (0) |
hi Danielle , I ma using Win XP sp2 , no ther siemens software are installed onthe PC. Which patch I have to use & onwhich I will get it. Regards |
8/13/2007 8:41 PM | |
Posts: 3149 Rating: (171)
|
Hi here the actual patch: http://support.automation.siemens.com/WW/view/en/25869221 nemo |