Industry Online Support
Technical Forum
5/3/2007 2:11 PM | |
Posts: 1275 Rating: (123)
|
Hi Balogh, Can't you switch to a Profibus-DP radio / gateway? This would be another solution, but you'd need a CP on the WinCC side. I found this post which mentions both CP243 and RS232/485 + PC Access software... This is on WinCC + DP + S7-200. This is on WinCC + Ethernet + S7-200. This is also on ethernet, and this FAQ. Some more on WinCC + S7-200. Here's how to acces S7-200 on WinCC. In the end all you need is to choose a protocol, and find a radio with it. Since the radio will only provide the media the protocol won't really matter. Remember that RS232 is only a physical standard to an interface, it's not a protocol. Best regards, Danielle |
5/3/2007 5:38 PM | |
Posts: 3149 Rating: (171)
|
Hi please find attached the possible ways of communication http://support.automation.siemens.com/WW/view/en/21915573 nemo |
Follow us on