4/7/2020 9:44 AM | |
Joined: 11/14/2018 Last visit: 4/3/2025 Posts: 502 Rating:
|
Hello Kristjan_, Just for completeness: In this thread (or further threads mentioned in it) you find a lot about text lists:
Does that mean, that you don't want to specify a specific, existing text list in a control, during engineering? As long a I can remember, it's not possible to 'change' text lists in runtime. But i may be wrong. You can try this:
I hope this get's you further Regards Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
4/9/2020 1:23 PM | |
Joined: 8/3/2009 Last visit: 4/23/2025 Posts: 15338 Rating:
|
Hello it depends on which HMI System you are using. If you have a Basic Panel-> no Way the dynamic textlists are not available. If you have Comfort/Advanced -> then look here: https://support.industry.siemens.com/cs/de/en/view/57025748 if you have a WinCC Professional Runtime Project then you can do a lot with Scripting... It would make things easier if you post all nessecary information at the beginnig of your topic.... Bye Murof |
Last edited by: Murof at: 04/09/2020 13:24:13If this Information really helps, you could use the Rate function |
|
Follow us on