Industry Online Support
Technical Forum
3/4/2008 11:26 PM | |
Posts: 2661 Rating: (279) |
Yes, you can use redundant terminal bus (6ES7652-0XX01-1XF0) with 2 network cards each on the clients and the servers. |
3/5/2008 1:16 PM | |
Posts: 60 Rating: (2) |
It seems a package with 2 designated network cards. Am I right? |
3/5/2008 5:55 PM | |
Posts: 2661 Rating: (279) |
Yes, the GT and the MT adapters. Two NIC's with a common IP address using "teaming". |
3/7/2008 2:44 PM | |
Posts: 60 Rating: (2) |
I checked it is used for PCS7. Is that mean the package needs PCS7 for configuration? |
Follow us on