Industry Online Support
Technical Forum
2/28/2008 11:18 AM | |
Joined: 12/8/2006 Last visit: 2/27/2020 Posts: 170 Rating:
|
hi anguraj, ---------------------------------- (1) wincc client server ---------------------------------- you need the "wincc server lizenz" in the case only if you have a wincc project type "Multi-User Project": wincc server <==> wincc clients (multi clients) ==> I believe in your case wincc server lizence is not necessary. ---------------------------------- (2) wincc opc-da server ---------------------------------- - wincc is delivered with opc-da server ("da" means data access). -Other applications can access the the WinCC-OPC-Sever via network without additional lizenses on the wincc server. - There is no special engineering necessary on the wincc server. The WinCC-OPC-Server provides all tags of wincc data manager automatically. But!!!! - It is very important, that you configure the windows operating system on the WinCC Server (OPC Server) - DCOM-Settings - Firewall - Group Policies ==> example http://support.automation.siemens.com/WW/view/en/15049230 |
Follow us on