9/29/2006 6:28 AM | |
Joined: 5/24/2006 Last visit: 11/14/2007 Posts: 93 Rating:
|
Hi Attached is a sketch on 2x reducdant Servers + 1x WinCC Client configuration which monitor and control both area 1 and 2. Following are some doubts of mine; [1] Can this configuration works? From WinCC Client HMI to control/monitor both area 1 & 2. [2] At PC5, can I configure such a way that user with access right of area 2, only can see itself? [3] With full access right at WinCC client (PC5), can I have FULL control in term of WinCC on both Server 1 and Server 2? [4] What if I need both servers to provide me information of the complete area 1&2, what should I do in PC5? I'm now having 2 different set of data archive servers? [5] How to minimise the re-engineering effort if area 1 is implementing now and area 2 is in later stage? [6] How many basic licences I need for this set of system? Attachment2 RedundantServers and 1 client.pdf (132 Downloads) |
Follow us on