7/30/2007 10:18 AM | |
Posts: 3149 Rating:
|
Hi please attach ALL files from folder ..\wincc\diagnose here in the forum. nemo |
7/30/2007 10:48 AM | |
Posts: 30 Rating:
|
Hi!! AttachmentDiagnose.zip (64 Downloads) |
7/30/2007 3:06 PM | |
Posts: 30 Rating:
|
Hi!! Thanks for answering, But i think u r reading some old diagnosis files which i've corrected recently. Andi knowi've to buy license for just temperory viewing of project butis this problem arising by running WinCC in demo mode. Please go through the diagnosis filesfrom around thistime2007-07-30 18:29:50. Can u help me out as i'm also unable to do communication with WinCC licensed PC with PN/DP PLC or CP5611 card. Regards, himexpert. AttachmentDiagnose.zip (35 Downloads) |
7/30/2007 10:21 PM | |
Posts: 1275 Rating:
|
Hi, Your logs are almost clean, then... they only show you had a connection problem. Have you made sure there are absolutely no tags in WinCC accessing DB positions, or DB's which haven't been created in the PLC (the PLC's DB's must be updated, and the WinCC tags must be poiting to the right places, all of them.. sometimes the DB's in the PLC are a little shorter than they should be)? To test this you can backup your project, and then delete all tags you've created on your last modification... If all you changed in that modification was adding tag logging, it shouldn't affect the communication... I found this FAQ regarding communication error codes... your code isn't there... Best regards, Danielle |
Follow us on