9/16/2016 8:30 AM | |
Joined: 3/20/2013 Last visit: 12/10/2023 Posts: 22 Rating:
|
Hello, Michael. Please see attached file with the installed software list. The OPC-server is local (installed on the same PC). To run Runtime I do not download the project to another path but just start the simulation. Then the OPC-server runs as a service and the connection to the remote unit is established (OPC-server receives data from the unit) Attachmentconfig.xlsx (316 Downloads) |
10/17/2016 4:17 PM | |
Joined: 3/20/2013 Last visit: 12/10/2023 Posts: 22 Rating:
|
In addition the WinCC V14 Runtime Prof. works correctly with the same adjustment as V13SP1. |
Follow us on