2/8/2024 9:33 AM | |
Joined: 8/3/2009 Last visit: 1/10/2025 Posts: 14538 Rating: (1812)
|
Hello TMBragg First idea is to work with AddressMultiplexing with symbolic addressing (you will need not scripts): https://support.industry.siemens.com/cs/ww/en/view/109815056/83078586123 The link is to the Comfort/Advanced Manual but works the same in Unified also. Then create two tag interfaces, one for the UDT ( not for the Array) and one for the index On the call of the Popup use an internal tag for the index (that you are also using for the multiplexing) and the multiplex tag for the UDT I have used this a lot of times already with Unified and it works good. Bye Murof |
Last edited by: Murof at: 02/08/2024 09:33:38If this Information really helps, you could use the Rate function |
|
Follow us on