11/14/2024 8:05 AM | |
Joined: 2/17/2020 Last visit: 2/13/2025 Posts: 1197 Rating:
|
Hi, Please see the sizing guidelines for the log and each segment on page 89 of the sample application below: Configuring Logging for SIMATIC WinCC Unified Systems With SQLite, the limit for log and segment size is limited by the underlying file system. Additionally, please note that SQLite allows a maximum of 5,000 logging tags, while SQL Server allows the maximum number of configurable PowerTags. Further information can be found here: SIMATIC HMI WinCC Unified V19 > Logging data - How it works |
A rating will be well appreciated. |
|
This contribution was helpful to
2 thankful Users |
Follow us on