7/30/2024 7:48 AM | |
Joined: 1/21/2013 Last visit: 4/17/2025 Posts: 3764 Rating:
|
Hi, The first thing you need to know is that you cannot change the color of a gif image. But you can import two images and switch between them. To know that the communication to the PLC is not running, you can use the quality code.
Kind regards |
9/24/2024 12:14 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello you can use define the timer in the global script area and start it for example at screen load and stop it if you have to ... More information about using timers you can see in the programming manual: https://support.industry.siemens.com/cs/ww/en/view/109896132/157858368651 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on