3/11/2021 11:51 AM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424)
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Sometimes it may be necessary to disable access to an application's controls, for example during screen cleaning operations. This function can be done in several ways, in this example it is done as follows:
Project archived and zipped Attachmentclear Screen.zip (729 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to6 thankful Users |
1/29/2024 9:15 AM | |
Joined: 4/28/2015 Last visit: 4/16/2024 Posts: 6 Rating: (0) |
Hi, as from TIA V19, a clear screen feature as added as system function (https://support.industry.siemens.com/forum/br/pt/posts/sample-and-tips-wincc-unified-activate-clean-screen/310573/?page=0&pageSize=10 ) |
This contribution was helpful to2 thankful Users |
Follow us on