7/11/2024 11:01 AM | |
Joined: 8/3/2009 Last visit: 9/13/2024 Posts: 13684 Rating: (1726)
|
Hello MZulDTM first of all try to configure all certificates and settings for the Runtime: https://support.industry.siemens.com/cs/de/en/view/109806850 Does this appear with every project/Simulation? Also if you start a new test Project? do you use the latest available Update (4) for V18 (engineering and runtime) Bye Murof |
Last edited by: Murof at: 07/11/2024 11:02:23If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
7/11/2024 11:18 AM | |
Joined: 1/21/2013 Last visit: 9/13/2024 Posts: 3096 Rating: (483)
|
Hi MZulDTM, Your traces show a stop of the WinCC Unified Datamanager due to an invalid or inconsistent RFD file. This can be caused by an unhandled error in the project, an error in the compiler or something else. You should make sure that you have installed the latest updates for both WinCC Unified Engineering and WinCC Unified PC Runtime. It may be that you just need to do a full compilation. It may help to delete the 'IM\HMI' folder within your TIA Portal project on your file system. However, if you cannot get rid of this error, you should contact technical support as a deeper look into your project may be necessary. Kind regards |
Follow us on