1/20/2025 3:05 PM | |
Joined: 2/17/2020 Last visit: 2/7/2025 Posts: 1188 Rating:
|
Hi, I suspect that it is not possible to store the Report directly on the shared path / network drive, since the manual states the following (see link): "You can use a network drive only for the data exchange between the server PC and HMI device. This means that a network drive cannot for example, be used for the following functions: - Updating, backing up and restoring the operating system - Transferring a project - Importing user management from a file or exporting it to a file - Runtime functions such as logging or reporting - Importing certificates". However, you could first store the Reports in a USB / SD storage medium inserted in the UCP, select the USB / SD as the path and then use the "copy.sh" script to copy the files from the USB / SD to the shared folder / network drive: Scripts for network drives and external storage media > copy.sh |
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
Follow us on