8/16/2012 12:33 PM | |
Posts: 21 Rating: (2) |
I cannot found my CP-TCP/IP in "Set PG/PC interface" option, I've click "Select" in add/remove interface to add the CP-TCP/IP but it wasn't there. |
8/16/2012 4:45 PM | |
Joined: 8/31/2010 Last visit: 1/24/2025 Posts: 1523 Rating: (230) |
Hello Dwayne Chou, Do not press Select under the Add/Remove Interface, rather choose the CP-TCPIP under the Access point of the Application at the top. As said earlier - Why does communication not work between WinCC Professional Runtime and S7-1200? |
Like it? Rate it! |
|
Follow us on