10/31/2016 2:49 PM | |
Joined: 5/12/2006 Last visit: 4/17/2025 Posts: 22597 Rating:
|
Hi, have you check the Windows Event Viewer if here mor information available?
Christoph |
11/2/2016 10:43 AM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello Aniki What do you want to do exactly?? Will you use WinCC Professional RT as OPC UA Client (then use the communication Channel at Connections) or do you want to use it as OPC UA Server (then you open Runtime Settings-> OPC Settings and edit the Configuration of OPC UA Server)? You wrote something about communication Channel and something about OPC Service... look at this FAQ here the WinCC Professional is a OPC UA Server: https://support.industry.siemens.com/cs/de/en/view/63481236 Bye Murof |
If this Information really helps, you could use the Rate function |
|
9/19/2017 7:33 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by Haydoo is split to a separate thread with the subject Issue with Downloading the OPC. Best regards |
Follow us on