6/13/2023 10:27 AM | |
Joined: 5/23/2022 Last visit: 11/11/2024 Posts: 1 Rating:
|
Hi, did you manage to solve it? I have the same problem but I have WinCC V17 for both aplicattions so it should be easier. I tried to copy data from the "ArchiveManager" folder but it didn't work. Could you help me? Thank you!
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/23/2023 10:48:51New subject after splitting. Quote inserted. |
|
6/15/2023 1:16 PM | |
Joined: 8/3/2009 Last visit: 4/29/2025 Posts: 15375 Rating:
|
Hello Marcos The data from Archive manager are not the complete archive. There are also taglogging and alarmlogging databayes in the root directory and they manage the whole database segments. here is a Link to a workaround for WInCC V7/8 where you can see what i mean, perhaps this helps also in case of your usecase: https://support.industry.siemens.com/cs/de/en/view/24193864 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on